BRU9950900-01

Padlocks

Padlock points are provided to help prevent unauthorized access to the unit.

Padlocks are used on the E/S and the disconnector.

Padlocks can be supplied upon request if specified at the time of enquiry or order.

CAUTION
LOSS OF PROTECTION HAZARD
Ensure the padlock used has a shackle diameter between 6 to 8 mm.
Failure to follow these instructions can result in injury or equipment damage.

Padlock on E/S or Disconnector

Earthing switch and the disconnector can be locked using the padlock.

NOTE: The main door and the LV compartment door can be locked by padlocks.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?