BRU9950900-01

Unpacking

All units are delivered on pallets (secured by 4 x M8 screws and nuts) and fitted with lifting lugs; suitable for off loading by forklift truck or overhead crane.

NOTE: Ancillary kits include cable boots, glands, screws, and so on. They are either packed loose with the unit or attached to the panel leg or cable boxes to help ensure all parts are ready for installation.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?