BRU9950900-01

Handling Instructions

WARNING
HAZARD OF EQUIPMENT TOPPLING
  • Wear appropriate PPE.
  • Keep the unit in vertical orientation while handling.
  • Handle the equipment with appropriate care as specified below.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
CAUTION
HAZARD OF INAPPROPRIATE HANDLING, STORAGE, and Installation
  • Respect the handling rules and avoid any shocks to the device.
  • Perform the maintenance and servicing operations described in the maintenance section of this guide. Refer to Maintenance.
  • Observe the normal service conditions described in this guide. Refer to Storage.
  • Ensure to lift the unit by using only lifting lugs, with all the four lifting points.
  • Do not stand/mount anything on the unit.
Failure to follow these instructions can result in injury or equipment damage.
CAUTION
HAZARD OF EQUIPMENT TOPPLING
Keep the equipment upright and handle with care. There is a tendency for the equipment to tilt due to its high center of gravity.
Failure to follow these instructions can result in injury or equipment damage.

The transport and handling information of Ringmaster AirSeT are as follows:
  • Units can be carried on open topped trucks or stored outside for short periods provided that all apertures are covered.

  • Units must not be considered weatherproof until the paintwork has been inspected, and if necessary, any damage must be repaired. Refer to Paintwork for repairing damaged paintwork.

  • For long-term storage, units should be kept in a warm, dry place, and protected from dust and debris.

  • The conditions and types of transport have been stipulated in the contract details.

  • The type of packaging depends on the type of transport and the storage conditions.

NOTE:
  • The Ringmaster AirSeT unit is suitable for outdoor storage if it is properly packaged.

  • The type of cable gland provided will depend on the specific contract requirements.

For detailed information, please refer to the commercial documentation included with the equipment package.

Lifting of Ringmaster AirSeT

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?