BRU9950900-01

Sizing of the Civil Engineering for Ringmaster AirSeT

The civil engineering dimensions apply specifically to the 3-function Ringmaster AirSeT unit. Refer to Figure – Positioning of Ringmaster AirSeT Unit from Wall.

Positioning of Ringmaster AirSeT Unit from Wall

L1

Recommended minimum clearance: 800 mm for safe operation, access and egress

P1

Depth of Trench

R

Curvature Radius of Cable

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?