BRU9950900-01

High Voltage Withstand Test

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Ensure that all VT primary connections are fully isolated before performing any HV pressure testing on the equipment.
  • When applying AC/DC test voltages greater than 12 kV, it is recommended to add supplementary insulation to the bushing to help prevent flashover or insulation failure.
  • The bushing sleeve is designed to be used in conjunction with some additional insulation method, such as econ boot or heat shrink termination boots.
Failure to follow these instructions will result in death or serious injury.

Connect the HV test set as shown in the Figure – Connections of Circuit Breaker/Switch and Figure – Schematic of Test Connection and carry out the withstand tests in accordance with the Table – Test Voltages and Table – Test Connection.

High Voltage Connection

Schematic of Test Connection

Test Voltages

Rated Voltage (kV)

AC Test Voltage (kV)

Frequency (Hz)

Duration (minutes)

DC Test Voltage Current Practice (kV)

3.6

8

50

1 (AC) 15 (DC)

7.5

7.2

16

50

1 (AC) 15 (DC)

15

12

23

50

1 (AC) 15 (DC)

25

Test Connection

Test Number

Ring Switch 1

Ring Switch 2

Circuit Breaker

Live Terminals

Earthed Terminals

1

Closed

Closed

Closed

L1, L3

L2, Frame

2

Closed

Closed

Closed

L2

L1, L3, Frame

3

Closed

Closed

Open

L1, L2, L3

L1, L2, L3, Frame

4

Closed

Closed

Open

L1, L2, L3

L1, L2, L3, Frame

5

Open

Open

Closed

L1, L2, L3

L1, L2, L3, L1, L2, L3, Frame

6

Open

Open

Closed

L1, L2, L3, L1, L2, L3

L1, L2, L3, Frame

Connections of Circuit Breaker/Switch

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?