BRU9950900-01

Disposal After the End of the Useful Life

A material and recycling data sheet can be provided on request for the disposal of Ringmaster AirSeT RMU at the end of its service life. Disposal is performed as a service by Schneider Electric service center which is subjected to payment.

This service is compliant with IEC 62271-200 standards, and conforms to local regulations. For more information, refer to end-of-life document ENVEOLI2505026.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?