BRU9950900-01

Functional Checks

Follow the below steps to perform the functional checks:

  1. Check the conformance of auxiliary switch contacts and remote indication in accordance with the schematic diagram.

  2. Confirm the phase relationship of the neon indicator sockets.

NOTE: All voltages must be applied instantaneously unless otherwise specified.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?