BRU9950900-01

Connecting the Integrated Cable Test Facility

WARNING
HAZARD OF INCORRECT OPERATION
Do not open the earth collector before connecting the test equipment.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Connecting the integrated Cable Test Facility

To set up the unit, proceed to the following steps:


Step 3:
Manually open the integrated cable test facility door.

Step 4: Manually (no tool) screw the 4 injection fingers (earth and 3-phases).

Step 5: Connect the cable from the test set to the injection fingers.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?