BRU9950900-01

Phase Concordance Unit

WARNING
HAZARD OF INCORRECT OPERATING CONDITIONS
Disable any automation which uses the voltage presence signal before carrying out the phase concordance test.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
NOTICE
HAZARD OF INCORRECT OPERATING CONDITIONS
  • After completing phase concordance testing, ensure the VDIS cover is reinstalled and securely clicked into position.
  • Ensure that each of the three cables is correctly connected to the corresponding phase of the Ringmaster AirSeT unit.
  • Phase concordance testing must be performed every time a cable is connected to the unit.
Failure to follow these instructions can result in equipment damage.

A phase concordance unit checks if the phases of two input units on the same panel match before turning on the switches. It help ensures that each of the three cables connects to the correct phase. The unit must follow the
IEC 62271-215:2021 standard.

Check Before Phase Concordance Test

Check that VDIS versions on each switch function allow the use of the phase concordance unit, refer to the below Table – Check Before Phase Concordance Test.

WARNING
HAZARD OF INCORRECT OPERATING CONDITIONS
Ensure phase concordance does not work between an I switch function and a Q earthing switch function.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

I switch function: Operation-independent opening or closing by lever or motor when operated electrically, an operation requires less than 10 s.

Q earthing switch function: Operation-independent opening or closing by lever. Operating energy is provided by a compressed spring which, when released, causes the contacts to open or close.

Check Before Phase Concordance Test

Test

Result

Action

Check that the three indicator lights of each VDIS are on.

The three indicator lights of each VDIS are on.

The two functional units are energized, the VDIS units are operating and the check can continue.

The three indicator lights of one VDIS are off. The functional unit is not energized or the VDIS is malfunctioning.

Apply power to the functional unit. If VDIS remains unlit, replace it.

If necessary, update VDIS so that both are the same version

One or two light indicators unlit.

The VDIS is inoperative, replace it. If necessary, update VDIS so that both are the same version.

Checking the phase concordance unit.

The phase concordance unit is defective.

Check the phase concordance unit. Refer to the Phase Concordance Unit User Manual.

A phase concordance unit cannot be used to test VPIS and VDIS. It will result in an indication of phase not in concordance.

Compatibility Test

Functional unit 1

Functional unit 2

Compatibility result

Corrective actions

Not OK

Upgrade unit to VDIS

Not OK

Upgrade unit to VDIS

OK

Phase Concordance Test

When all three indicator LEDs on both VDIS units are lit, it means the phase concordance unit is working correctly and the phase test can be carried out.

The phase concordance unit complying with IEC 62271-215: 2021 standard should work well. Taking phase concordance unit with phase concordance light as shown in below Table – Phase Concordance Test.

  • Phase concordance: the phase concordance light remains unlit.

  • No phase concordance: the phase concordance unit light is lit.

Phase Concordance Test

Phase Concordance Test

Functional unit 2

Conclusion regarding phase concordance

L1

L2

L3

Functional unit 1

L1

Connection is satisfactory.

L2

L3

Functional unit 1

L1

Reverse the MV cables connected to L1 and L2 on one of the two functional units.

L2

L3

Functional unit 1

L1

Reverse the MV cables connected to L2 and L3 on one of the two functional units.

L2

L3

Functional unit 1

L1

Reverse the MV cables connected to L1 and L3 on one of the two functional units.

L2

L3

Functional unit 1

L1

Change the position of each MV cable on one of the two functional units.

L2

L3

Functional unit 1

L1

Change the position of each MV cable on one of the two functional units.

L2

L3

Phase concordance unit LED lights

LED unlit

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?