Handling Instructions of VIP Relays
The handling instructions for the VIP installed on the Ringmaster AirSeT are as follows:
-
Handling: Handle the equipment with appropriate care, check the VIP condition by visual inspection and energizing.
-
Transport: VIP relays can be transported by all suitable means of transport in the usual conditions for unit.
Storage conditions should be taken into consideration for a long period of transport. -
Storage: It is recommended to keep the VIP in its original packaging for as long as possible to help protect the unit during storage.
VIP relays, like all electronic devices, should not be stored in humid or damp conditions for more than one month. The relay should be powered up as soon as possible after installation to maintain optimal performance. If immediate energization is not possible, the unit reheating system must be activated to help prevent moisture-related damage.
LED Status Indicators
The status LEDs indicators provide information about the VIP general status. For details, refer to the below Table – VIP Status Indication.
VIP Status Indication
Fault Indication LEDs
The VIP relays have fault indication LEDs. They flash to indicate a fault, refer to the below Table – VIP Fault Indication.
VIP Fault Indication
Following a trip event, the fault indication LEDs are powered either by the internal battery embedded in the VIP unit or, in the case of the VIP 410, by its auxiliary power supply.
The fault indication LEDs can be reset using one of the following methods:
-
Manual Reset: Press the Reset key on the front panel of the VIP unit.
-
Automatic Reset: The LEDs reset automatically when there is reappearance of a current in the network higher than the pick-up current. The LEDs reset automatically 24 hours after the trip event.
-
Remote Reset (VIP 410 only): The LEDs can be reset via remote control order through communication.