BRU9950900-01

Sizing of the Civil Engineering for Network Switch

The civil engineering dimensions apply specifically to the 3-function Ringmaster AirSeT unit. Refer to Figure – 3-Function Ringmaster AirSeT Unit.

Cables can be routed from both the left and right sides, depending on site layout.

3-Function Ringmaster AirSeT Unit

P1

Depth of Trench

R

Curvature Radius of Cable

NOTE: The depth of trench is determined based on cable bending radius specifications and it should withstand unit weight.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?