BRU9950900-01

Safety Precautions

You are responsible for compliance with all the existing international and national electrical codes concerning protective grounding of any device.

You should also carefully read the safety precautions described below. These instructions must be followed strictly when installing, servicing or repairing electrical equipment.

DANGER
HAZARD OF ELECTRICAL SHOCK, EXPLOSION, OR ARC FLASH
  • Only qualified personnel should install this equipment. Such work should be performed only after reading the instructions as per this manual.
  • Never work alone.
  • Turn off all power supplying this equipment before working on or inside it.
  • Always use a properly calibrated voltage sensing device to confirm power is off.
Failure to follow these instructions will result in death or serious injury.
WARNING
HAZARD OF INAPPROPRIATE OPERATION
Before performing visual inspections, tests, or maintenance on this equipment:
  • Disconnect all sources of electric power.
  • Assume that all circuits are live until they have been completely de-energised, tested and tagged.
  • Beware of potential hazards, wear personal protective equipment, and carefully inspect the work area for tools and objects that may have been left inside the equipment.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?