BRU9950900-01

Floor Preparation Test

The non-extensible units can be directly bolted to the concrete floor by use of
4 x M10 (supplied) UNI-FIX or similar rag bolt fixings. The floor tolerance for the unit is ±1 mm over 1 m.
For details refer to Figure – Switchboard Bolt Tolerance.

Switchboard Bolt Tolerance

A

Foot of unit

B

M10 channel fixing

C

Floor level flush to +/-1 mm with foundation channel

D

Spring loaded channel nut

E

Channels made in subfloor

F

Channels grouted in position using setting jigs supplied

NOTE: If the floor does not meet the specified tolerance, it is highly recommended to use foundation channels, such as Unistrut P3270 or similar. The floor should be 1 mm below the top of the Unistrut.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?