BRU9950900-01

Packaging

NOTICE
HAZARD OF INCORRECT HANDLING
  • Qualified personnel must handle the lifting of the unit.
  • It is recommended to use the inspected cranes or the forklift for transportation.
  • The lifting or the handling of the unit from the loaded transportation vehicle should be done accordingly to the safety guidelines.
  • Carefully disassembly of the packaging is essential to prevent damage to the unit.
Failure to follow these instructions can result in equipment damage.

The packaging for various modes of transportation are as follows:

  • If packed exclusively for truck transport, the units are delivered on a pallet with Polyethylene (PE) protection film.

  • For sea transport, the units are packed in sealed aluminum foil with desiccant and in a closed wooden case with tightly closed wooden base (also for container transport).

  • In case of air transport, the units are packed in wooden crates with protective PE film hood (dust protection) or in wooden crates, also with closed wooden bases, however without protective hoods.

NOTE: Observe the center of gravity label to help ensure proper transport. You can find the label on the packaging and on the equipment.

Transport the Package with Forklift Truck

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?