BRU9950900-01

Interlocks

The Ringmaster AirSeT complies with the recommendations of IEC 62271-200 and as per ENA 41-41 for functional interlocks and integrates a set of built-in native robust mechanical interlocks in each function.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?