BRU9950900-01

Transport

WARNING
HAZARD OF EQUIPMENT TOPPLING
  • When transporting the unit, ensure that the units do not tilt or tip.
  • Nail down transport pallets to the loading surface.
  • For transporting the trucks, comply with the transport specifications in the appropriate manuals.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
CAUTION
HAZARD OF EQUIPMENT TOPPLING
  • The entire length of the forks must be placed under the transport unit.
  • When handling forklift truck, keep the unit as close as possible from its vertical position. There is a tendency for the equipment to tilt due to its high center of gravity.
Failure to follow these instructions can result in injury or equipment damage.

All units can be off loaded by a forklift truck using the transport pallet. They can also be off loaded using the lifting lugs fitted at the top of the unit with addition of the strap to avoid the damage of the equipment during the transit position.

Transport with Forklift Truck

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?