BRU9950900-01

Different Types of Bushings

There are two different types of bushings fitted in the Ringmaster AirSeT unit, they are:

  1. Switch bushing.

  2. CB bushing.

Switch Bushing

CB Bushing

Switch bushing type C is made to fit 50 mm Current Transformer (CT) from Schneider Electric and most CTs used in fault indicators.

CB bushing type C is made to fit 50 mm or 90 mm CTs from Schneider Electric and most CTs used in fault indicators.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?