BRU9950900-01

General Characteristics

The Ringmaster AirSeT is an indoor and outdoor MV secondary distribution switchgear or Smart RMU MV Gas-Insulated switchgear applications up to 12 kV 630 A designed for durability and ease of use. It comes with an IP54 rated enclosure and a stainless steel tank rated IP67.

Its simple mimic layout supports user-friendly operation, while the type C bushing options provide compatibility with a wide range of third-party termination systems.

The switchgear includes interlocked access for MV cable testing, allowing safe testing procedures without the need to disconnect the cable terminations.

Additionally, it features integrated self-powered protection for transformers or network monitoring, and supports direct coupling to transformers or cable connections, simplifying both installation and maintenance.

The Ringmaster AirSeT provides optional features as follows:

  • Facilities for electrical operation.

  • Electrical tripped on-fault indication.

  • Range of dry type metering units.

  • Remote monitoring and control through PowerLogic T300 range of Feeder Remote Terminal Units (FRTU).

For more information, contact Schneider Electric.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?