BRU9950900-01

Mechanical Interlocks

The Ringmaster AirSeT mechanical interlocks are intended to help avoid some incorrect operations.

The operation of the interlock mechanism on the switchgear is applicable for:

  1. VCB and disconnector.

  2. Cable test facility of RS1 and RS2.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?