BRU9950900-01

Housing

Exterior

Follow the below steps to inspect the exterior of the unit:

  • Check all the external fixings and labels are present, and the earth connections are tight.

  • Check the main door and cable box for the heavy deposits of dust, ingress of water or contamination by animal or plant life.

  • Clean the units thoroughly and touch up paint work as necessary.

Interior

Follow the below steps to inspect the interior of the unit:

  • Open the main door.

  • Check that the gas indicator is in the green zone.

  • For circuit breaker unit check the electrical protection system.

  • Check the operation of the unit and all mechanical interlocks.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?