BRU9950900-01

Manual Spring Charging of VCB

Follow the below steps for manual spring charging:

  1. Pull down the spring charging handle until the VCB is fully charged.

  2. After the spring is charged, VCB is ready to be closed.

  3. To close the VCB, press the closing push button.

  4. To open the VCB, press the opening push button.

  5. The disconnector mechanism can be operated only when VCB is in OFF position.

NOTE: There is an interlock between VCB and disconnector which helps to prevent the operation of disconnector when the VCB is in ON position.

Manual Spring Charging of Circuit Breaker

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?