BRU9950900-01

Discharging the Cables to the Earth

Discharging the Cables to the Earth

To set up the unit, proceed to the following steps:

Step 1: Ringmaster AirSeT A.

Open the main switch and padlock.

Step 2: Ringmaster AirSeT B.

Open the main switch and padlock.

Verify if the cable is out of voltage. If no, refer to the network operator company.

Close the earthing switch and padlock it.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?