Configurations
The Ringmaster AirSeT is available in three different configuration:
-
RN2 AIR TLF/VIP Standalone - AF.
-
RN2 AIR TLF/VIP TX Mounted - AF.
-
RN2 AIR TLF/VIP Standalone - AF - T300.
|
1 |
Disconnector/Switch Mechanism |
7 |
Right ring switch cable box |
|
2 |
VCB |
8 |
Remote terminal unit - T300 |
|
3 |
Voltage and Current Protection (VIP) 400/410/45 Relay |
9 |
LV Box |
|
4 |
Manometer |
10 |
Left ring switch cable box |
|
5 |
Ring Switch 2 (RS2) Mechanism |
11 |
Operating handle |
|
6 |
Ring Switch 1 (RS1) Mechanism |
12 |
Voltage Detecting and Indicating System (VDIS) |