BRU9950900-01

Door Stopper

Locking the door stopper

Door stopper will lock once the main door is opened at desired angle and the door stopper locks itself by gravity, refer to Figure – Door Stopper.

Unlocking the door stopper:

Lift the door stopper by hand to unlock it and close the main door, refer to Figure – Door Stopper.

Door Stopper

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?