BRU9950900-01

Internal Arc Diverter Plate

Follow the below instruction to assemble the internal arc diverter plate on the Ringmaster AirSeT after installing the cable connection:

  1. Install the internal arc diverter plate (1) when attaching the cable box cover.

  2. Mount the internal arc diverter plate (1) on the rear side of the unit, following the orientation as shown in Figure – Internal Arc Diverter Plate for Transformer Configuration.

  3. Install six quantities of M8 x 25 Hex. bolts and torque the bolts to 20 N•m.

Internal Arc Diverter Plate for Transformer Configuration

1

Internal Arc Diverter Plate

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?