VIP 45
VIP 45 is a protection relays with a self-powered supply. VIP 45 is powered by their current sensor and operate without an auxiliary power supply.
-
The VIP 45 can be used for protection against phase faults and earth faults.
-
VIP 45 displays current measurement.
Presentation
The UMI on the front panel of VIP relays consists of a display, LEDs and keys. A protective flap helps to prevent access to the setting keys by unauthorized persons.
|
1 |
Display |
7 |
Status LED |
|
2 |
Lugs for opening the transparent protective flap |
8 |
Space for a user-customizable label |
|
3 |
Transparent protective flap |
9 |
Trip fault indication LED |
|
4 |
Imax. peak demand display button |
10 |
Identification label |
|
5 |
Sealing ring |
11 |
Read manual symbol |
|
6 |
Test/Reset button |
12 |
Battery |
Identification Label
The identification label on the front panel enables a VIP 45 to be identified.
|
1 |
Product name |
|
2 |
Product reference |
|
3 |
Serial number |
VIP 45 Settings
When the protective flap is opened, you can enter the protection settings by means of the rotary switches. To do this, use a 3 mm flat blade screwdriver.
To set the protection settings, follow the below steps:
-
Open the protective flap on the VIP 45 unit.
-
Use the rotary switches to enter protection settings.
-
Use a 3 mm flat-blade screwdriver to do the adjustment.
|
1 |
Phase overcurrent protection adjustment dial |
5 |
Advanced settings protective cover |
|
2 |
Setting range selector switch |
6 |
Connection port for the pocket battery module |
|
3 |
Earth fault protection set point adjustment dial |
7 |
Trip test button |
|
4 |
Earth fault protection time delay adjustment dial |