BRU9950900-01

Delivery

CAUTION
HAZARD OF INAPPROPRIATE ASSEMBLY
In the event of any anomaly or apparent damage, do not install, contact Schneider Electric.
Failure to follow these instructions can result in injury or equipment damage.
NOTICE
HAZARD OF INAPPROPRIATE STORAGE CONDITIONS
The functional unit must remain on its base, in its original packing. In the event of an anomaly, contact the transport/shipping company.
Failure to follow these instructions can result in equipment damage.

Shipping units must be checked upon receipt as follows:

  • Inspect the equipment carefully for damage or loss incurred during transit, before accepting.

  • Check the presence of accessories against the packaging list.

  • Check the information on the nameplate(s) and compare against the order confirmation.

  • The packing must be in place and in good condition at the time of receipt. Any damage which may have occurred in transit must be recorded and reported to the manufacturer immediately.

NOTE: It may be necessary to unpack the equipment to establish the full extent of the problem.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?