BRU9950900-01

Mission Profile

The standard operating conditions of mission profile are defined by IEC 62271-1. For mission profiles or environmental conditions not covered by this standard, contact Schneider Electric.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?