BRU9950900-01

Essential Checks

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Do not operate this equipment if the needle is in the red zone or at zero, refer to pressure check.
  • Isolate and earth the equipment before removing any external covers.
  • The option of VDIS must be used as indication only. It should not be used as absolute proof of isolation.
  • Never earth a live cable which is energized from a remote end.
  • Check voltage of the respective CB/switch before operating the unit.
  • Prior to operating the CB/switch, ensure the manometer needle is in green zone.
Failure to follow these instructions will result in death or serious injury.
WARNING
HAZARD OF INAPPROPRIATE OPERATION
  • Before energizing the unit, ensure all protection devices are correctly set.
  • Ensure that fuses are fitted for TLF units.
  • VIP units must be set in accordance with the results of a protection co-ordination study.
  • Short the current transformers (T300 and earth fault flow indicator) that are not going to be used during commissioning or during service.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Manometer

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?