BRU9950900-01

Manual Operation of Motorized Ring Switch

The motorized ring switch can also be manually operated as follows:

  1. Make sure that the ring switch is in OFF position and the green motor selector is ON Motor (M) position.

    Ring Switch is in OFF position

  2. Rotate the shutter knob in the clockwise direction.

    Rotating the Green Motor Selector

  3. While still holding the shutter knob, push and rotate the green motor selector in anti-clockwise direction to non-motorized position, refer to the Figure – Green Motor Selector in Non-motorized Position.

    Green Motor Selector in Non-motorized Position

  4. While still holding the shutter knob, take out the green motor selector to gain access for operating handle.

    Removal of Green Motor Selector

  5. CAUTION
    HAZARD OF INAPPROPRIATE OPERATION
    The padlock should be locked only when the green motor selector is removed and the ring switch is in OFF condition.
    Failure to follow these instructions can result in injury or equipment damage.

Padlock on Ring Switch

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?