BRU9950900-01

Paintwork

NOTICE
HAZARD OF EQUIPMENT CORROSION
  • Make sure the unit surface is clean and free from any paint damage.
  • If any damage is found, repaint the affected areas. For detailed instructions, refer to the procedure below.
Failure to follow these instructions can result in equipment damage.

Check for any damaged paintwork. Damaged areas must be cleaned and re-coated as follows:

  • Rub down the area around the damage with medium glass paper.

  • Clean the damaged area with emery paper, to help ensure the surface is clean and free of any corrosion.

  • Apply one coat of zinc-rich epoxy primer (a two-pack system is recommended), the coating to be 35–45 microns thick.

  • Leave to cure for 24 hours, then apply two 35–45 micron coats (that is, 60–80 microns in total) of two-pack polyester paint. Interphane PFR 764 is recommended.

NOTE: The additional recommended paint system is international paints Interzinc EPA 072 and EPA 073. The standard color employed is Dark Grey RAL7012.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?