BRU9950900-01

Rating Plate

The type designation on the rating plate specifies the technical data of the Ringmaster AirSeT. To access this information, flash the QR code with smartphone or connected tablet; it will be directed to the website containing the data relating to the device.

When submitting enquiries to the manufacturer or ordering spare parts, the following information is required:

  • Type designation

  • Job number

Rating Plate


1

Type designation

3

Technical data

2

Job number

4

QR code with product information

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?