Safety Provisions
Introduction
Before performing work on the unit, it is essential that you comply with the following instructions: DANGER |
|---|
|
HAZARD OF electric shock, explosion, or arc flash
Before removing covers and performing assembly or maintenance
work:
Failure to follow these instructions will result in death or serious injury.
|
WARNING |
|---|
|
HAZARD OF MOVABLE PARTS IN MECHANICAL DRIVES
Before performing mounting and maintenance work, comply
with the below safety rules:
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
WARNING |
|---|
|
HAZARD OF SHARP-EDGED SHEET METAL AND METAL PARTS
During installation and maintenance work, comply with
the below safety rules:
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
Applicable Standards and Regulations
The applicable standards and regulations are as follows:
Applicable Standards and Regulations
|
Description |
IEC standard |
|---|---|
|
Switchboard |
IEC 62271-200 IEC 62271-1 |
|
Behavior in the event of internal faults |
IEC 62271-200 |
|
Earthing switch |
IEC 62271-102 |
|
Ring switch |
IEC 62271-103 |
|
Circuit breaker |
IEC 62271-100 |
|
Current transformer |
IEC 61869-2 |
|
Voltage transformer |
IEC 61869-3 |
|
Voltage presence indication system |
IEC 62271-206 |
|
Voltage detection and indication system |
IEC 62271-213 |
|
Protection against accidental contacts, foreign bodies and ingress of water |
IEC 60529 |
|
Basic and safety principles for man-machine interface, marking and identification |
IEC 60445 |
|
Ground mounted distribution substation RMU and Extensible switchgear (Rated 12–24 kV) |
ENA TS_41-41_301197 |
-
Comply with the national standards applicable in the country where the equipment is to be installed.
-
Other standards or regulations have to be checked and accessed locally.
Environmental and Operating Conditions
The operating conditions for the installation of standard Ringmaster AirSeT unit to meet the normal service conditions are as defined by IEC 62271-1, clause 4.1.3. Refer to the below Table – Environmental Specifications.
Environmental Specifications
|
Environmental Specifications |
Values |
|---|---|
|
Ambient Air Temperature |
≥ -25 °C to ≤ +45 °C |
|
≤ +35 °C on average over 24 hours |
|
|
Surface Temperature |
≤ +60 °C |
|
Altitude |
≤ 1000 m above sea level(1) |
|
Solar Radiation |
≤ 1000 W/m2 |
|
Ambient Air Pollution |
Site Pollution Severity (SPS) class medium as defined by IEC TS 60815-1: 2008 |
|
Ice Coating |
≤ 20 mm |
|
Wind Speed |
≤ 34 m/s |
|
Absolute Humidity |
Relative humidity can reach 100% when absolute humidity is 30 g/m3, leading to possible precipitation or condensation. |
|
Rain Intensity |
≤ 15 mm/m with a driving rain < 18 m/s |
|
(1) At higher altitudes, de-rating might be necessary according to the functional units and/or the installation altitude. For more information, refer to Installation Altitude. |
|
Behavior in Case of Incidents
In the event of an internal arc fault, theRingmaster AirSeT unit is equipped with pressure relief flaps or exhaust ducts designed to help safely vent the resulting gases.
This operation and maintenance manual guide does not include information regarding the safety of buildings in case of internal faults (pressure load of the unit room and necessary pressure relief flaps). Pressure calculations for the unit rooms, including recommendations for pressure relief ducts, are available upon request for a fee. For more information, contact the licensed partner or Schneider Electric.
In case of fire or internal faults, toxic and caustic decomposition products are produced. Comply with the locally applicable safety provisions.
Make sure that the first-aid measures are taken in case of injury to persons.
DANGER
WARNING