BRU9950900-01

Operating Handle

CAUTION
HAZARD OF INAPPROPRIATE OPERATION
  • The operating handle must only be operated on the switches, when the front plate is installed.
  • Only use the genuine operating handle provided by Schneider Electric to operate the switch manually.
  • The operating handle must be completely inserted before operating.
Failure to follow these instructions can result in injury or equipment damage.

The operating handle is a mandatory accessory for the Ringmaster AirSeT unit and for operating the switch/disconnector mechanism and the earthing switch.

Operating Handle

NOTE: The operating handle is supplied with the Ringmaster AirSeT unit.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?