BRU9950900-01

Opening and Closing the Ringmaster AirSeT Main Door

CAUTION
HAZARD of inappropriate operation of door handle
Ensure the handle is rotated in accordance with the operating instructions provided below.
Failure to follow these instructions can result in injury or equipment damage.

Opening the Main Door:

  1. Insert the key into the handle lock to unlock the door handle.

  2. Rotate the handle 90° anti-clockwise to open the door, refer to the below Figure – Opening and Closing the Ringmaster AirSeT Main Door.

Closing the Main Door:

  1. Make sure that the handle is in the door open position.

  2. Press the door firmly against the fascia, then rotate the handle 90° clockwise to help secure it, refer to the below Figure – Opening and Closing the Ringmaster AirSeT Main Door.

Opening and Closing the Ringmaster AirSeT Main Door

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?