BRU9950900-01

Safety Precautions

Safety Rules

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Apply appropriate Personal Protective Equipment (PPE) and follow safe electrical work practices.
  • This Ringmaster AirSeT equipment must only be installed and serviced by qualified electrical personnel.
  • Perform work only after reading and understanding all of the instructions contained in this guide.
  • Turn off all the power supplies of the equipment before working on or inside the equipment.
  • Respect the LOTO (Lock Out Tag Out) procedure.
  • Always use a properly calibrated voltage sensing device to confirm power is off.
  • Put all devices, doors, and covers back into place before turning on power to this equipment.
  • Beware of potential hazards, and carefully inspect the work area for tools and objects that may have been left inside the equipment.
  • Depending on the internal arc classification, it is recommended to not access the rear or sides of the switchgears when it is energized.
  • Do not modify the mechanical or electrical parts.
  • Do not bypass the interlocks before operation.
Failure to follow these instructions will result in death or serious injury.
NOTICE
Hazard of inappropriate handling and storage
  • Comply with the handling rules and avoid causing any shocks to the device.
  • If the equipment is stored before its final installation, observe the storage conditions.
Failure to follow these instructions can result in equipment damage.

Cleaning Instructions

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Do not use solvents or alcohol for cleaning the equipment.
  • Do not use high-pressure cleaner for cleaning the equipment.
Failure to follow these instructions will result in death or serious injury.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?