BRU9950900-01

Connection of MV Cables

WARNING
Hazard of inappropriate assembly
Follow the below instructions before connecting the high voltage cables and all connections:
  • All connections must be made according to the manufacturer’s instructions.
  • Ensure the equipment is firmly secured to the ground.
  • Connect the Ringmaster AirSeT frame to the main earth bar (refer to Figure – Main Earth Bar).
  • Ensure that the earthing switch of cable box bushings is in the ON position.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
NOTE: Access to the bushings for the switch provided on the lateral sides, and for the circuit breaker at the rear side.

Main Earth Bar

1

Main Earth Bar

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?