BRU9950900-01

Interlocks for Integrated Cable Test Facility of RS1 and RS2

The logic for operating the cable test facility and cable test switch (RS1 and RS2) based on the current state of the unit is shown in the below Table – Ringmaster AirSeT Interlocks with Cable Test Facility and Cable Test Switch (RS1 and RS2).

Ringmaster AirSeT Interlocks with Cable Test Facility and Cable Test Switch (RS1 and RS2)

Ringmaster AirSeT Interlocks with Cable Test Facility and Cable Test Switch (RS1 and RS2)

Logic position of functional unit

Position before operation

Operation wished

Switch

Cable test facility

Close the switch

Open the witch

Close the E/S

Open the E/S

Close the cable test access

Open the cable test access

ON

Closed

Closed

OFF

Open

Closed

Earthed

Earthed

Closed

Earthed

Earthed

Open

Free

Locked

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?