BRU9950900-01

Protection Relays

All circuit breakers can be fitted with various forms of protection system. In the Ringmaster AirSeT the VIP (Voltage and Current Protection) self powered Inverse Definite Minimum Time (IDMT) protection relays are used.

The different types of VIP protection relays used in the unit are as follows:

  • VIP 400.

  • VIP 410.

  • VIP 45.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?