BRU9950900-01

Pressure Check

The manometer installed on the Ringmaster AirSeT unit indicates the pressure inside the unit. There are different zones indicated on the manometer.

Follow the below mentioned cases to understand the pressure checks as follows:

Case 1: Needle in Green Zone

If the needle is in the green zone, the Ringmaster AirSeT unit can be operated normally.


Case 2: Needle in Green Shaded Zone

If the needle is in the green shaded zone, the Ringmaster AirSeT unit can be operated. However, this indicates that there is an abnormal leakage, contact the Schneider Electric.

Case 3: Needle in Red Zone

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
If the needle is in red zone, do not make any operation on Ringmaster AirSeT unit. Contact the Field Service representative immediately.
Failure to follow these instructions will result in death or serious injury.

If the needle is in the red zone, the Ringmaster AirSeT unit should not be operated. There is an abnormal leakage level, contact the Schneider Electric.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?