BRU9950900-01

Interlocks for VCB and Disconnector

The logic for operating the VCB and disconnector based on the current state of the unit is shown in the below Table – Ringmaster AirSeT Interlocks with VCB and Disconnector.

Ringmaster AirSeT Interlocks with VCB and Disconnector

Ringmaster AirSeT Interlocks with VCB and Disconnector

Logic position of functional unit

Position before operation

Operation wished

Disconnector

VCB

Close the disconnector

Open the disconnector

Close the E/S

Open the E/S

Close the VCB

Open the VCB

ON

Closed

Closed

OFF not disconnected

Closed

Open

OFF and disconnected

Open

Open

Earthed

Earthed

Open

Earthed

Earthed

Closed

Free

Locked

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?