SUG_Wiser_Russia_WSE-02

Dimmers

Connected Universal Push-Button Dimmer LED

Controls the lighting level in a room, or automatically set lighting to a desired level in response to a specified condition or event.

Instruction Sheet (PDF)

Device User Guide

Connected Universal Rotary Dimmer LED

Instruction Sheet (PDF)

Device User Guide

Connected Motion Sensor with Universal Push-Button Dimmer LED

Controls the lighting level in a room, or automatically set lighting to a desired level in response to detected motion, a specified condition or other event.

Instruction Sheet (PDF)

Device User Guide

Wiser Micro Module Dimmer

Converts compatible mechanical push-button switches into smart dimmers. Connect up to 10 compatible mechanical push buttons.

Примечание: Mechanical push buttons must be certified for use in 220–240 V AC applications.

Instruction Sheet (PDF)

Device User Guide

Обратная связь
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.