Archive Services Console

Use the console to manage your existing instances of Archive Services. By default, the Configuration screen is displayed. Click the link to Console to manage your Archive Services.

If you are running multiple instances of Archive Services, there will be multiple console windows (one for each instance). To use a command, enter it in the Input field and click Send. The results of the command are displayed in the windows for each Archive Services instance running. The various commands you can use in this window are listed in Responder Services Commands.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.