TmScenarios Table
|
Field |
Description |
|---|---|
|
Scenario |
A unique number identifying the scenario. This field is a primary key. |
|
Name |
A description for the scenario. |
|
Device Facility ID |
The Facility ID of the outage device. |
|
Device Type |
The Type of the outage device. |
|
DeviceFcid |
Feature class ID for the incident device. |
|
DeviceOid |
Object ID for the incident device. |
|
Customers Affected |
The number of customers affected by the outage. |
|
NumberCalls |
The number of customers that called in the scenario. |
|
NumberHazards |
The number of hazards in the scenario. |
|
Comments |
Comments about the outage. |