Modify Domain Values
You may modify the domain values displayed in Responder Explorer drop-downs using the DatabaseSchemaConfig.xml file.
In the example below, "Tidal Wave" was added to the list of options in the Weather field on the Edit Incident tab. Changes to DatabaseSchemaConfig.xml do not go into effect until DataServices.exe has been restarted. To use a different value other than one provided in the domain by default, we recommend creating a new value (see note) and deleting the existing value.
Before modifying domain values:
<Domain Name="WEATHER" xsi:type="CodedDomainConfig" DataType="Int32">
<DomainPair Value="0" Description="<Unknown>" />
<DomainPair Value="1" Description="Hurricane" />
<DomainPair Value="2" Description="Ice Storm" />
<DomainPair Value="3" Description="Other" />
<DomainPair Value="4" Description="Snow Storm" />
<DomainPair Value="5" Description="Thunderstorm" />
<DomainPair Value="100" Description="Tidal Wave" />
<DomainPair Value="6" Description="Tornado" />
<!-- Domain Values 7-99 are RESERVED FOR SCHNEIDER ELECTRIC USAGE!! -->
</Domain>
Before modifying domain values:
The following table contains a complete list of Responder domains. Some domains may NOT be modified and some domains have values that must not be modified. These are indicated.
|
Domain |
Used by |
Notes |
|---|---|---|
|
ACCOUNT_TYPE |
Indicates the type of client account (e.g., hospital, residential, industrial) |
Modify any values in this domain. |
|
CALL_TROUBLE |
Problem reported at the incident location (e.g., No Power, Flickering Lights). |
Do not modify the following values: 0=No Power, 5=<None>, 6=Other. All values except 0 are assumed to have at least some power (e.g., flickering). 0 is the only "no power" type value. |
|
CALLBACK_REASON |
Reason for the callback to the customer. |
Modify any values in this domain. |
|
CALLBACK_RESULT |
The result of the last callback attempt (e.g., wrong number, left message). |
Do not modify the following values: 0=Call Completed, 3=No Answer, 4=Busy Signal, 5=Power NOT Restored, 6=Delete Callback. |
|
CANCEL_REASON |
Indicates the reason for cancelling an incident. |
No not modify the following value: 0=Unknown |
|
CAUSE |
Indicates the cause of the outage. This is the default domain. If you run the Reliability Indices: SAIDI by Cause Code Report OR Minutes and Outage Count by Cause Code Report with CAUSE_RUS domain values, the following message appears: There was at least one Incident Cause value that did not match to a value in the specified domain. |
Do not modify the following values: 0=Unknown, 6=Planned Outage, 10=Non-Outage |
|
CAUSE_RUS |
Indicates the cause of the outage. An alternate domain created for RUS Bulletin 1730A-119. |
Do not modify the following values: 0=Unknown, 6=Planned Outage, 10=Non-Outage, 1=Power Supply |
|
CLOSED_PHASES |
Indicates the actual status of the incident device (e.g., AB open). |
You may edit the values in this domain, but do not change the meaning. For example, AB closed may become XY closed. But changing AB closed to X open will cause faulty behavior. |
|
CONNECT_STATUS |
Indicates the connection status for the customer (e.g., connected, disconnected) |
Do not modify the following values: 0=Connected - normal, 1=Connected - seasonal. You may add values only for various types of disconnected status. |
|
CREW_ASSIGNMENT_STATUS |
Indicates the status of a crew's assignment (e.g., unassigned, dispatched, working). |
Do not modify the 0=Unassigned value. You can change the remaining values, and you can change the meaning or add/remove as many statuses as desired between ‘Assigned’ and ‘Completed.' You cannot, however, change the meaning of ‘Assigned’ and ‘Completed.' |
|
CREW_AVAILABILITY_STATUS |
Indicates the availability of a crew (yes/no). |
You may edit the values in this domain, but do not change the meaning (e.g., Available, Meal Break, Unavailable). |
|
CREW_COMPANY |
The name of the company to which the crew belongs. |
Modify any values in this domain. |
|
CREW_TYPE |
The type of crew (e.g., company, contractor). |
Modify any values in this domain. |
|
CRITICAL_TYPE |
Indicates the type for accounts designated as critical (e.g., residential medical, public utility). |
Do not modify the following value: 0=Non-critical. All values except 0 are considered critical. |
|
EXPERTISE |
Indicates the expertise for a crew member (e.g., lineman, foreman). |
Modify any values in this domain. |
|
HAZARD_TYPE |
The type of damage at a hazard location (e.g., wires down, broken pole). |
Modify any values in this domain, except 2=Wires Down. You may edit this value, but do not change the meaning. |
|
HAZARD_WIRE_OWNER |
Owner of the wire on which the hazard resides (e.g., phone, CATV). |
Modify any values in this domain. |
|
NETWORK_LEVEL |
Indicates the network level. Network level is a custom grouping set up by an administrator (e.g., primary, secondary, transmission, supply). |
Refer to Configure Network Level Field topic for value modification details. |
|
ORIGINATION_TYPE |
This field indicates how the incident was created (e.g., User Created, Predicted, SCADA). |
You may add values to this domain (values 100 and above). Do not modify the existing values. You may, however, change their visibility. |
|
PHASES |
Indicates the phase (e.g., A, AB, BC). |
You may edit the values in this domain, but do not change the meaning. For example, AB may become XY. But changing AB to X will cause faulty behavior. |
|
PRIORITY_TYPE |
Indicates the customer's priority (e.g., hospital, business center). |
Do not modify the following value: 0=Non-priority. |
|
SWITCH_ORDER_REQUEST_STATUS |
Indicates status of a switch order request (e.g., created, approved, assigned). |
You may edit the values in this domain, but do not change the meaning. |
|
TAG_ACTION |
Indicates what's being done to the tag (i.e., place or remove). |
You may edit the values in this domain, but do not change the meaning. For example, "Remove" may be changed to "Eliminate". |
|
TAG_TYPE |
Indicates the type of tag being placed (e.g., Do Not Operate, Do Not Open). |
Do not modify the following values: 1=Do Not Operate, 2=Do Not Close, 3=Do Not Open, 5=Do Not Energize. |
|
TITLE |
The job title associated with a crew member (e.g., Crew Leader, Electronic Tech). |
Modify any values in this domain. |
|
TRUCK_COMPANY |
This domain provides a list of companies that may own trucks. |
Modify any values in this domain. |
|
TRUCK_STATUS |
Indicates the availability status of a truck. All values except 0 are considered non-operational. 0=Operational, 1=Non-Operational |
You may edit the values in this domain, but do not change the meaning of 'Operational' (0). All values other than 0 are considered non-operational. |
|
TRUCK_TYPE |
Indicates the type of truck assigned to the crew (e.g., bucket truck, line truck). |
Modify any values in this domain. |
|
UTILITY_TYPE |
Indicates the type of utility (e.g., electric, water, gas). |
Modify any values in this domain. |
|
VOLTAGE_VALUES |
Indicates the voltage of the device (e.g., < 1 KV, 25 KV, > 60KV). |
Modify the sort order of this domain by changing the SortedBy attribute to one of the following:
|
|
WEATHER |
The weather conditions at the time of the outage (e.g., tornado, snow storm). |
Modify any values in this domain. |
|
IMPORTANT: Do not modify the following domains. Responder functionality
relies on these domains to remain unchanged.
|
||
|
CALLBACK_STATUS |
Indicates the status of a customer callback (Regular Call/Power Not Restored Call). |
Do not modify any values in this domain. |
|
CALLER_TYPE |
Indicates the source of the call (e.g., IVR, CSR). |
Do not modify any values in this domain. If you do modify the values in this domain, the changes will not be visible in the Responder web application. |
|
CONFIRMED_STATE |
Indicates the confirmation status of an incident (confirmed/unconfirmed). |
Do not modify any values in this domain. |
|
CRITICAL |
Indicates whether an incident is critical or not (yes/no value). |
Do not modify any values in this domain. |
|
DEVICE_FCID |
Dynamic domain |
Do not modify any values in this domain. |
|
DEVICE_OPERATION |
Indicates whether an operations is a fault (unplanned outage) or a switching operation (planned outage). |
Do not modify any values in this domain. |
|
FCID |
Dynamic domain |
Do not modify any values in this domain. |
|
HAZARD_STATUS |
Indicates the status of the hazard (e.g., unsecured, secured, completed). |
Do not modify any values in this domain. |
|
INCIDENT_CHILD_TYPE |
Indicates the type of feature associated with an incident (e.g., electric feature, location feature, hazard). |
Do not modify any values in this domain. |
|
INCIDENT_DURATION |
The length of time an incident exists. |
Do not modify any values in this domain. |
|
INCIDENT_STATUS |
Indicates the status of an incident (e.g., created, restored, cancelled). |
Do not modify any values in this domain. |
|
OPEN_CLOSED |
Indicates whether a device is opened or closed. |
Do not modify any values in this domain. |
|
OPERATION_STATUS |
Indicates the status of the operation (e.g., not executed, executed). |
Do not modify any values in this domain. |
|
OPERATION_TYPE |
Indicate the type of operation (e.g., Custom, Tag, Device). |
Do not modify any values in this domain. |
|
ORIGINATION_TYPE |
The source of the incident (e.g., User Created, Predicted). |
Do not modify any values in this domain. |
|
OWNER |
Dynamic domain |
Do not modify any values in this domain. |
|
OWNER_STATE |
The status of the feature owner (e.g., no owner, pending, approved). |
Do not modify any values in this domain. |
|
REGION |
Dynamic domain |
Do not modify any values in this domain. |
|
SWITCHING_ORDER_STATUS |
Status of a switching order (e.g., created). |
Do not modify any values in this domain. |
|
SWITCHING_ORDER_TYPE |
Indicates a switching order or restoration order. |
Do not modify any values in this domain. |
|
TAG_ORIGINATION |
Indicates how the tag was created (e.g., manual, switching order). |
Do not modify any values in this domain. |
|
YES_NO |
A general yes/no domain. |
Do not modify any values in this domain. |