RX_INCIDENT_DEVICE_STEPS
|
Field Name |
Description |
|---|---|
|
OPERATION_ID |
The ID field from RX_OPERATIONS (foreign key). |
|
EXPECTED_STATUS |
The expected or normal status of the device (open, closed). |
|
PLANNED_STATUS |
The planned status of the device (e.g, Open, Closed). |
|
PLANNED_CUSTOMER_COUNT |
The number of customers affected by a planned step. This value indicates a net change in the number of energized customers. It will be either a positive number (power restored to customers) or negative number (customers losing power). |
|
PLANNED_CRITICAL_COUNT |
The number of critical customers affected by a planned step. This value indicates a net change in the number of energized customers. It will be either a positive number (power restored to customers) or negative number (customers losing power). |
|
PLANNED_CONNECTED_LOAD |
Amount (in kVA) by which the total system connected load will change due to the planned step. |
|
EXECUTED_CUSTOMER_COUNT |
The number of customers affected by an executed step. This value indicates a net change in the number of energized customers. It will be either a positive number (power restored to customers) or negative number (customers losing power). |
|
EXECUTED_CRITICAL_COUNT |
The number of critical customers affected by an executed step. This value indicates a net change in the number of energized customers. It will be either a positive number (power restored to customers) or negative number (customers losing power). |
|
EXECUTED_CONNECTED_LOAD |
Amount (in kVA) by which the total system connected load will change due to the executed step. |
|
USER_CREATED |
The name of the user who created the record. This field is populated automatically by Responder. |
|
USER_UPDATED |
The name of the user who updated the record. This field is populated automatically by Responder. |
|
ACTUAL_STATUS |
The current actual status of the device (open, closed). |
|
ACTION |
The action to be taken by the operation (e.g., open, close). |
|
PHASES |
The phase(s) to be operated by the step. |