RX_OPERATIONS_ARCHIVE
|
Field Name |
Description |
|---|---|
|
OPERATION_ID |
This field corresponds to the ID field in the RX_OPERATIONS table. |
|
ORDER_ID |
The ID associated with a switching order. This field corresponds to the ID field in the RX_SWITCHING_ORDERS table. |
|
INCIDENT_ID |
The ID associated with the incident. This field corresponds with the ID field in the RX_INCIDENTS table. |
|
SEQUENCE |
The sequence number of the operation (the step number in the switching order). |
|
TYPE |
Indicates the type of operation (custom, tag, or device). |
|
DESCRIPTION |
Description of the operation (e.g., "Open", "Remove Ground", "Place Tag"). |
|
FCID |
Feature class ID of the feature associated with the tag. |
|
OID |
Object ID of the feature associated with the tag. |
|
SUBID |
The unique ID of each segment of a complex edge. |
|
X |
The x-coordinate of the incident device. |
|
Y |
The y-coordinate of the incident device. |
|
FACILITY_ID |
The Facility ID of the incident device as defined in the geodatabase. |
|
SUBSTATION_ID |
The ID of the substation that feeds the incident device. |
|
FEEDER_ID |
The Feeder ID of the incident device. |
|
OPERATION_STATUS |
Indicates whether the operation has been executed, not executed, or cancelled. |
|
EXECUTED_BY |
User name of the person who executed the operation. |
|
TIME_EXECUTED |
The time the operation was executed. |
|
OWNER_STATE |
This field tracks the state of a switching operation with regard to an external owner of a device. This field uses the Owner_State domain. |
|
TIME_OWNER_APPROVED |
This field tracks the time of approval by an external owner of the device (e.g., OASyS). |
|
REMARKS |
Notes from the operator or dispatcher. |
|
USER_CREATED |
The name of the user who created the record. This field is populated automatically by Responder. |
|
USER_UPDATED |
The name of the user who updated the record. This field is populated automatically by Responder. |
|
CHANGE_DATE |
The time and date an operation was performed on the record. |
|
OPERATION |
The operation (e.g., insert, delete, update) performed on the record. |
|
USER_UPDATED_ARCH |
This field is not currently used by Responder. You may customize Responder to populate this field with the name of the user who updated the record. |
|
EXECUTED_BY_NAME |
The name of the user who executed the switching order operation. |
|
LINE_TYPE |
Indicates the type of operation (e.g., open close, tag, etc.). |
|
SUMMARY |
Any summary comments included by the user on the switching order operation. |
|
FEATURE_CLASS_NAME |
The name of the Feature Class on which the incident occurred, as it was configured/named when the Incident was archived. |
|
PARENT_SEQUENCE_ID |
This value acts as a group number when grouping operations within a switching order. All operations in the same group share the same PARENT_SEQUENCE_ID. |