RX_CUSTOMERS_ARCHIVE
|
Field Name |
Description |
|---|---|
|
ACCOUNT |
The customer's account number. |
|
ACCOUNT_TYPE |
Indicates the type of account. Uses the Account_type domain. |
|
METER |
The customer's meter number. |
|
FIRSTNAME |
The customer's first name. |
|
LASTNAME |
The customer's last name. |
|
STREET |
The customer's street address. |
|
CITY |
The customer's city. |
|
STATE |
The customer's state. |
|
POSTAL_CODE |
The customer's zip code. |
|
COUNTY |
The customer's county. |
|
TELEPHONE |
The customer's telephone number. |
|
TELEPHONE2 |
An alternate telephone number for the customer. |
|
TELEPHONE3 |
An alternate telephone number for the customer. |
|
TELEPHONE4 |
An alternate telephone number for the customer. |
|
CALLBACK_NUMBER |
Preferred number for contacting the customer. |
|
DEVICE_OID |
The object ID of the device to which the customer is associated (e.g., service point or transformer). This field links to the OID field in your geodatabase. |
|
DEVICE_FCID |
The feature class ID of the device to which the customer is associated (e.g., service point or transformer). This field utilizes the DEVICE_FCID domain. |
|
REGION |
The region in which the customer is located. This field uses the REGION domain. |
|
CONNECT_STATUS |
Indicates the status of the user's connection (connected/disconnected). This field uses the CONNECT_STATUS domain. |
|
TIME_DISCONNECT |
Indicates the time the customer was disconnected. |
|
TIME_RECONNECT |
Indicates the time the customer's power was reconnected. |
|
CRITICAL |
Indicates if the customer site is critical. This field uses the CRITICAL_TYPE domain. |
|
PRIORITY |
Indicates if the customer site is priority. This field uses the PRIORITY domain. |
|
USER_CREATED |
The name of the user who created the record. This field is populated automatically by Responder. |
|
USER_UPDATED |
The name of the user who updated the record. This field is populated automatically by Responder. |
|
USER_UPDATED_ARCH |
This field is not currently used by Responder. You may customize Responder to populate this field with the name of the user who updated the record. |
|
FEATURE_CLASS_NAME |
The name of the Feature Class on which the incident occurred, as it was configured/named when the Incident was archived. |
|
CHANGE_DATE |
The time and date an operation was performed on the record. |
|
OPERATION |
The operation (e.g., insert, delete, update) performed on the record. |