RX_PREVIOUS_INCIDENTS_ARCHIVE

Field Name

Description

TIME_OUTAGE

The time the outage occurred.

TIME_RESTORED

The time the customer's power was restored.

DURATION

Indicates the weather at the incident site. This field uses the WEATHER domain.

CHANGE_DATE

The time and date an operation was performed on the record.

HAZARD

Indicates any hazards in the area (e.g., fire, wires down, etc.). This field uses the HAZARD domain.

CAUSE

Indicates the cause of the outage. This field uses the CAUSE domain.

WEATHER

Indicates the weather at the incident site. This field uses the WEATHER domain.

INCIDENT_ID

The ID associated with the incident. This field corresponds with the ID field in the RX_INCIDENTS table.

REMARKS_DISPATCH

Remarks from the dispatcher.

REMARKS_FIELD

Remarks from the field crew.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.