RX_CREW_ASSIGNMENTS
| Field Name | Description | 
|---|---|
| INCIDENT_ID | Indicates the ID of the incident to which the crew has been assigned. This field is a foreign key to the RX_INCIDENTS table. | 
| CREW_ID | Indicates the ID of the crew that has been assigned to the incident. This field is a foreign key to the RX_CREWS table. | 
| STATUS | Indicates the status of the crew. This field uses the STATUS domain. | 
| TIME ASSIGNED | The time the crew was assigned to the incident. | 
| IS_LEAD_CREW | Indicates whether the crew is the lead crew. This field uses the IS_LEAD_CREW domain. | 
| USER_CREATED | The name of the user who created the record. This field is populated automatically by Responder. | 
| USER_UPDATED | The name of the user who updated the record. This field is populated automatically by Responder. | 
| TIME_STATUS_CHANGED | This is the time that a crew's status was changed (e.g., from Dispatched to Working) after it was modified by a dispatcher. | 
| PREVIOUS_TIME | This is the original time that the crew's status was set. | 
| MOBILE_CREW_ENABLED | A value that indicates whether the crew has been assigned a Mobile status. |